An eVTOL doesn't get a second chance if one power path falters mid-transition from vertical lift to forward flight, which is why the airframe is built around dual coverage from the start. The XMC7K24CA XClamp™ protection diode from Vishay absorbs up to 7 kW peak transient power to keep a surge on one path from cascading into the other. The IHCM-2321AA-10 common mode choke adds 1500 VDC of isolation between coils. Two paths, one airframe, no compromise.
Behind every vertical liftoff is The DNA of tech.®
This is our general contact form. If you have more specific questions or needs please select from the options below.